Search FAQs
Is a keypad included with ATV61 and ATV71 drives?
Issue:
Does the keypad come with ATV61 and ATV71 drives?
Product line:
ATV61, Altivar 61, ATV71, Altivar 71
Environment:
All models, all serial numbers
Cause:
Customer wants to know if they need to order a keypad separately.
Resolution:
All ATV61 and ATV71 drives include an integral simplified LED display and programming keys on the face of the control board. Any drive part numbers without a Z suffix will also include the VW3A1101 LCD keypad as standard. It can be mounted directly on the drive control board face or remotely. Part numbers with a Z suffix will not include the LCD keypad.
“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)“
Does the keypad come with ATV61 and ATV71 drives?
Product line:
ATV61, Altivar 61, ATV71, Altivar 71
Environment:
All models, all serial numbers
Cause:
Customer wants to know if they need to order a keypad separately.
Resolution:
All ATV61 and ATV71 drives include an integral simplified LED display and programming keys on the face of the control board. Any drive part numbers without a Z suffix will also include the VW3A1101 LCD keypad as standard. It can be mounted directly on the drive control board face or remotely. Part numbers with a Z suffix will not include the LCD keypad.
“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)“
Released for:Schneider Electric UK
Explore more
Explore more