{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the functions of the Telefast ABE7CPA412 sub-base?

The ABE7CPA412 Advantys Telefast sub-base is used as a wiring interface for BMXART0414 and BMXART0814 M340 automation platform thermocouple modules.

It is used to:
  • connect 4 thermocouple probes
  • perform external cold junction compensation using the temperature sensor integrated in the sub-base and ensure continuity of shielding.
Note: The BMXART0814 module requires 2 ABE7CPA412 Advantys Telefast sub-bases.