Search FAQs
How can I simulate an application on XBTH, XBTP or XBTE with XBTL1000 without PLC?
In order to simulate an application for a Magelis XBT-H , XBT-P or XBT-E using the XBTL1000 without being connected to a PLC we need:
1) Open the Configuration > Dialogue Table
2) Uncheck the "Use Dialogue Table"
3) Click on "OK"
4) Open the Simulation > Simulation Application
5) Enter address 0 when simulation asks you to.
It is now possible to display the page sequences without getting the error code "Cannot write table".
1) Open the Configuration > Dialogue Table
2) Uncheck the "Use Dialogue Table"
3) Click on "OK"
4) Open the Simulation > Simulation Application
5) Enter address 0 when simulation asks you to.
It is now possible to display the page sequences without getting the error code "Cannot write table".
Note: This platform is discontinued. Please get access to our digital catalog https://digicat.se.com/ or contact our support center for more information about migrations to a newer platform. |
Released for:Schneider Electric UK
Explore more
Explore more