Search FAQs
What Schneider Electric Drive has replaced the Telemecanique Altivar 58 (ATV58)
There have been several revisions of drives since the ATV58 was made obsolete. Therefore, it is best to consider the requirements afresh.
The current range that mat be acceptable is the ATV600 or ATV900 or in some cases the ATV320 or ATV340.
Either download the catalogue for the ranges range to find a suitable drive or contact Schneider Electric and we will assist you in selection
If you need support in selection it would be useful to have the following information available:
- Motor kW or HP rating?
- Motor Voltage?
- Motor Current?
- Application (eg Machine, Pump, Fan etc)?
- Load type or Torque Requirements (Variable or Constant)?
- Input voltage and number of Phases?
- Any communication protocols required?
This is not an exhaustive list, but will assist in directing to a suitable replacement or new drive.
Originally the recommended replacement for the ATV58’s where the the ATV71’s or ATV61 series drive but as these drives are now Obsolete the current ranges to choose from are the ATV320,340,600 and 900 series drives.