{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What replaced XPSAS? What are the differences between XPSAS and the new XPSAF?

NOTE that XPSAF has now been replaced by XPSUAF. Please see attached document for further information.

XPS-AS Replaced by XPS-AF
XPSAS (old model)                                             XPSAF (new model)
XPSAS (old model)                                             XPSAF (new model)
  • XPS-AF has one extra N/O safety output
  • XPS-AF is 22.5 mm width
  • XPS-AS has larger range of voltage selection
  • XPS-AS can be used for Type III A two-hand control monitoring
  • XPS-AF has choice between 2 models with or without removable plug terminals (P)
  • Schematic Comparisons
    Monitoring of E-stop with 2N/C contacts

    Monitoring of E-stop with 2N/C contacts
    Monitoring of E-stop with 1N/C contact

    Monitoring of E-stop with 1N/C contact
    Monitoring of E-stops with 2N/C contacts in series

    Monitoring of E-stops with 2N/C contacts in series
    Monitoring of a movable guard associated with 2 limit switches with 1 contact each

    Monitoring of a movable guard associated with 2 limit switches with 1 contact each
    Cross Reference Table

    Cross Reference Table
    NOTE: Data sheets about new safety relays XPSAF are available on the web site to download, use the search engine (top right corner)

Schneider Electric UK

Attachment(s)

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.