Can the C60H RCBO be used on a 110V AC System
A 110V version of the C60H RCBO is available which is suitable for use on a standard 0 - 110V AC TN-S earthing system
If the 110V AC supply is 55 -0- 55V AC, the C60H RCBO must not be used because it only switches 1 pole.
A suitable circuit breaker would be a 2 pole C60H MCB plus the add-on 2 pole Vigi mode.
Answers which others found helpful |