What is the recommended load for electronic dimmable transformers?
The minimum lamp loading of the transformer should be adhered to ensure efficient operation when dimming electronic transformers .It is recommended that electronic dimmable transformers be loaded to at least 70% of their rated maximum wattage.
This is due to the transformers inherent capacitance being increased at low loads, when in series with the dimmer this can reduce the overall capacitance of the circuit which may in turn reduce the stability of dimmer.
Answers which others found helpful |