Search FAQs
What are the maximum number of fault current operations Ringmaster and GenieEvo will clear?
The number of faults that a circuit breaker can clear will depend on the level of fault current being interrupted.
Ringmaster: -
Ringmaster: -
- 16kA - the circuit breaker is designed to clear a maximum number of 11 times at 16kA fault current
- 21kA - the circuit breaker is designed to clear a maximum number 10 times at 21kA fault current
GenieEvo is designed to clear a maximum of 100 faults at 25kA.
The fault current rating of the unit is detailed on the unit rating plate.
Released for:Schneider Electric UK
Explore more
Explore more