Can I convert a program from a TSX17 PLC into a program for TWIDO PLC?
No, it is not possible to convert a program from a TSX17 PLC to a Twido program.
The program must be re-entered.
FA28133 |
14-Feb-2011
|
Programming
PDF
Email
Bookmark
Print
Answers which others found helpful
> Which PLCs are programmed using the PL7-2 software?
> What is the part number of the transfer cable between a PC and a TSX17?
> Is it possible to program a Twido PLC through the 499TWD01100 TwidoPort Ethernet TCP/IP interface module?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel