FAQ Search

What is the substitution of the GSKC product by the XPSAK module?

The equivalent of the GSKC safety module used for emergency stop monitoring in accordance with standard EN954-1 category 4 is the XPSAK module. 

For applications with contacts in series running over long wiring distances, you must check beforehand, that the wiring resistance is less than the maximum value given in the catalogue for the XPSAK.

FA28074  |  05-Mar-2014  | Product Substitution
Please rate the content of this information
Unhelpful star.gif 1 star.gif 2 star.gif 3 star.gif 4 star.gif 5 Helpful
What can we do to improve this information?
Your email address