Can I place a TeSys U starter-controller downstream from a variable speed drive?
TeSys U controllers fitted with an LUCLxxxx control units are ideal for protecting drive/motor or starter/motor assemblies, but can only be installed upstream of the drive, not downstream.
If protection is required downstream of the drive, an LRD thermal overload relay must be used.
For further information on LUCL*** control units see the attached document.
If protection is required downstream of the drive, an LRD thermal overload relay must be used.
For further information on LUCL*** control units see the attached document.
Attachment(s):
Answers which others found helpful |