FAQ Search

Does the TSX Micro PLC have process control functions?

Yes.
The control loops are designed in a simple, user-friendly way using the 3 functions integrated in the PL7 Micro/Junior/Pro software:

  • The PID function used to perform a mixed PID correction (series - parallel)
  • The PWM function used to perform time modulation adaptations on discrete outputs
  • The SERVO function used to perform motor control adaptations


In an application for TSX37, the PID control functions must be programmed.
They are available in the PL7 function library.
Assistance with entering the PID function is available from the language editors, providing help with programming the function.

Note:
The TSX 37 does not have "LOOP" channels like those on Premium.

FA27923  |  14-Feb-2011  | Programming
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful