What safety functions are available with the XPSMC controller?
The XPSMCWIN software is used to configure 30 safety functions on the XPSMC controller.

They are certified in accordance with category 4 of standard EN954-1, PLe of EN ISO 13849-1, and SIL3 of IEC 61508.
The main safety functions are as follows:
single and dual channel emergency stop button with or without time delay
single or dual channel safety guard with or without interlock
solid state and relay output light curtains (type 4) with or without muting
magnetic switch
two-hand control device (type IIIC in accordance with EN 574)
safety mat
zero speed detection
injection moulding machine
hydraulic press valve monitoring (3 valves)
eccentric press control
OR logic
Enabling device
Attachment(s):
Answers which others found helpful |