FAQ Search

What is the syntax of the IP address in a READ_VAR or WRITE_VAR block in Unity Pro with an M340?

The syntax for indicating the IP address of the Modbus TCP/IP device to which the READ_VAR or WRITE_VAR function is to communicate is as follows: ADDM('network_link{HOST_ADDRESS}') Example: ADDM('Ethernet_1{192.100.200.120}') Illustration:



FA23718  |  25-May-2011  | Programming
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful