The main load on an Ulti switch / dimmer is turned off automatically
Possible causes are
1. The Power rating is too low. Replace the load with one that meets the minimum loading requirement.
2. Wires are not properly secured in the terminals. Make sure the wires are secured and screws are fastened properly.
3. The switch / dimmer is controlled by other remote control unit within the area. Determine which remote control unit(s) is (are) controlling the particular main light.
Answers which others found helpful |