What are the tripping times of the SM6 range products?
For SM6 switches (IM, PM or QM type cubicle):
The average response times depend on the type of operating mechanism used with the switch:
- 1 to 2 seconds on closing and opening for a motorised CIT operating mechanism
- 5 to 7 seconds on closing and 25 to 35 ms on opening for a motorised CI1 operating mechanism
- 45 to 55 ms on closing
- 25 to 35 ms on opening for a motorised CI2 operating mechanism after setting.
Reminder: The switch can only break a current corresponding to its nominal current, i.e. 400 A or 630 A. For SM6 circuit breakers (DM1A, D or W type cubicle): after setting the operating mechanism, the average response times of the SF1 circuit breakers are: 70 ms for closing. 50 to 60 ms for opening. Reminder: The circuit breaker can break a short-circuit current of 12.5 kA rms.
Answers which others found helpful |