FAQ Search

What is the part number of the Modbus RJ45 - USB adapter used in industrial control?


Part number VW3A8117 is an RJ45-USB adaptor, which can be used to connect ATV21, ATV31, ATV61, ATV71 drives to a PC via its USB port

This link allows the drive parameters to be transferred to the PowerSuite software workshop and vice versa.
 

The PowerSuite software workshop for PC is a user-friendly tool designed for setting up control devices for the following Schneider Electric products:

TeSys U starter-controllers
TeSys T motor management system
Altistart soft start - soft stop units
Altivar variable speed drives
Lexium 05 servo drives

It includes various functions designed for setup phases such as:

Configuration preparation
Start-up
Maintenance
In order to simplify the start-up and maintenance phases, the PowerSuite software workshop can use the Bluetooth® wireless link.

FA22892  |  25-May-2011  | Miscellaneous
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful