FAQ Search

Are the TSXETZ410 / TSXETZ510 modules compatible with the Premium PLCs?

No, the TSXETZ410 and TSXETZ510 modules are not compatible with Premium, Quantum or Twido PLCs.

They are only compatible with TSX Micro PLCs (with operating system version V2.0 or later), except TSX37-05 and TSX37-08.
These modules come with a TSXETZCDN003 Unitelway connection cable (length 0.35 m) and have an external 24 VDC power supply.
FA22859  |  11-Feb-2011  | Networking
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful