FAQ Search

What cable diameters can be used to connect foot switches?

Two types of cable can be used:

  • 6 mm to 10 mm diameter cables (1)
  • 10 mm to 14 mm diameter cables (2)

The cable clamp supplied with the product is reversible and can be used with both types of cable. Simply turn over the upper part of the cable clamp.

FA22725  |  11-Feb-2011  | Technical Documentation
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful