What address to use for TSXETZ410 and TSXETZ510? Set an address of a TSXETZ410 and TSXETZ510.
This FAQ is to alert users NOT to set the IP address on any of theses devices of 255.255.255.255.
Do not use this IP address, there is a risk of becoming non-functional, and the need of factory repair.
Answers which others found helpful |