FAQ Search

What replaced XPSAPF? What are the differences between XPSAPF and the new XPSAR?

XPS-APF replaced by XPS-AR

 XPSAPF (old model)                                                    XPSAR (new model)


  • XPS-AR has 2 extra solid state outputs for PLC signalling
  • XPS-AR has choice between 2 models with or without removable plug terminals (P)
  • XPS-AR has 1 extra N/O safety outputs
  • XPS-AR cannot monitor safety mats or edges
  • XPS-APS could be used for Type III A two-hand monitoring

Schematic Comparisons

Monitoring of E-stop with 2N/C contacts
 


Cross Reference Table


NOTE: Data sheets about new safety relays XPSAK are available on the web site to download, use the search engine (top right corner)
 
See also FAQ number FA141626
FA141633  |  07-May-2012  | Cabling and Connection
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful