Search FAQs
What size cables can be terminated into NSX100-250 MCCBs?
Compact NSX MCCB types NSX250, NSX160 & NSX100 accept cables up to 95mm2 using crimp lugs.
The lug sizes are:
NSX100 is M6
NSX160 and NSX250 is M8
If terminating 120, 150 or 185mm cables then cable spreaders and/or the reduced crimp lugs should be used. This is based on a single core Cu cables.
The lug sizes are:
NSX100 is M6
NSX160 and NSX250 is M8
If terminating 120, 150 or 185mm cables then cable spreaders and/or the reduced crimp lugs should be used. This is based on a single core Cu cables.
Released for:Schneider Electric UK
Explore more
Range:
Explore more
Range: