FAQ Search

Can I add additional contacts to an XD2G Joystick?

No, it is not permissible to add additional contact blocks to the XD2G Joystick controllers
However, if you have one contact in each direction, we do manufacture a unit with two contacts per direction.

There are two other alternatives to add additional contacts:
  • Replace the XD2G the an XKDF Joystick range, this has more contacts per movement.
  • Use an additional relay such as a Tesys CAD32** or Zelio Relay RXZ***
FA132999  |  23-Feb-2011  | Technical Characteristics
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful