FAQ Search

What are the differences between T200I and T200E

Functionally there are no differences between the two RTU's.

The key differences are: -

  • IP rating of T200I is IP41
  • IP rating of T200E is IP54
  • T200E is limited to controlling 4 functions
  • T200E can control up to 16 functions
  • T200I has Harting type connectors underneath the cubicle for the switchgear umbilical's
  • T200E has special sockets inside the cubicle on the interface card


For more information on T200I click here and T200E click here

FA132874  |  16-Jun-2011  | Technical Documentation
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful