FAQ Search

Can I have remote operation with my RM6

Remote operation is archived by integrating a RTU (Remote Telemetry Unit) such as T200I or T200E and fitting actuators to the required functions. It may also be necessary to add additional wiring looms to enable the RTU to be integrated and commissioned prior to putting it back into service.

For more information on:  -

FA132871  |  16-Jun-2011  | Operating System
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful