What is the maximum earth loop Impedance Zs value for the NS1600b to 3200 MCCB fitted with Micrologic trip units
The maximum earth loop Impedance figures can be found on the attached pdf file.
Attachment(s):
Trip settings NS 1600-3200A Micrologic.pdf
(PDF,115K)
FA132570 |
16-Feb-2011
|
Technical Documentation
PDF
Email
Bookmark
Print
Answers which others found helpful
> What is the maximum earth loop impedance Zs value for NS 630 b to 1600 MCCB with Micrologic trip units
> What is the maximum earth loop Impedance Zs value for the circuit breakers used in the Safepact range of enclosed MCCB's
> The NSX MCCB trips as soon as it's switched on and the display indicates ENCT or STOP
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel