Are the C60H miniature circuit breakers sold in the UK UL approved
The standard C60H offered in the UK is not UL approved.
However, we do offer various ranges of C60 devices that comply with UL 1077 or UL 489 standards.
Choosing the correct circuit breakers complying with UL standards can be complicated. Therefore we recommend that you contact technical support on 0870 608 8 608
However, we do offer various ranges of C60 devices that comply with UL 1077 or UL 489 standards.
Choosing the correct circuit breakers complying with UL standards can be complicated. Therefore we recommend that you contact technical support on 0870 608 8 608
Answers which others found helpful |