FAQ Search

What is the part number of the pushbutton mechanical interlocking device used in the XACA pendant control stations?

The part number of the mechanical interlocking device (mechanism) mounted between two pushbuttons on the XACA pendant control stations is;


It is possible to mount one XACA009 between each pair of buttons, e.g. between raise and lower. 3 way interlocking is not possible.

FA33169  |  08-Jun-2011  | Options and Accessories
Please rate the content of this information
Unhelpful star.gif 1 star.gif 2 star.gif 3 star.gif 4 star.gif 5 Helpful
What can we do to improve this information?
Your email address