FAQ Search

Can the cables used with XY2CH and XY2CE emergency stop trip wire switches be turned through angles or must they be straight?

The cables used to operate  XY2CHxxx and XY2CExxx emergency stop cable pull switches may be installed turning through angles by using the specified pulleys (XY2CZ708).The total sum of all the angles through which the trip wire bends must not exceed 180°.    





Caution: Part numbers XY2CBxxx must not be used if the installation requires the trip wire to be angled.
FA28127  |  14-Feb-2011  | Cabling and Connection
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful