How can I order other sets of keys for the 30 mm dia. selector switches of the Harmony 9001 range?
Harmony 9001 range selector switches, part numbers:
can only be ordered with the following keys:
No other keys are possible, as is the case for Harmony XB4 or XB5 pushbutton controls.
To obtain a set of spare keys:
- 9001KS11KxR
- 9001KS43K5R
- 9001KS53K5R
can only be ordered with the following keys:
- Ronis No.455
- E10 (US standard)
No other keys are possible, as is the case for Harmony XB4 or XB5 pushbutton controls.
To obtain a set of spare keys:
- For Ronis No.455 keys, order the part number from the catalogue for a set of 2 keys: ZBG455.
- For E10 keys, for which there is no part number in the catalogue, the following details must be specified to the Schneider Electric supplier-distributor: Reference: 2941101100