How can I distinguish thermal from magnetic faults when using GV2ME, GV2P, GV2L and GV2LE?
Using a GVAM11 combined with a GVAD10xx, it is possible to distinguish between thermal and and magnetic faults.
If there is no fault:
- GVAM11: contact 05-06 is closed and contact 05-08 is open
- GVAD10xx: fault contact 97-98 is open
- No LED is lit
If there is a magnetic fault:
- GVAM11: contact 05-06 is open and contact 05-08 is closed
- GVAD10xx: fault contact 97-98 is closed
- The short-circuit LED is lit, and the trip LED is off
If there is a thermal fault
- GVAM11: contact 05-06 is closed and contact 05-08 is open
- GVAD10xx: fault contact 97-98 is closed
- The trip LED is lit, and the short-circuit LED is off
Test for correct operation
The instantaneous auxiliary contact test is performed by creating a state of transition of the handle actuator between the de-energised position and the energised position.
The fault contact test is performed by pressing the test button when the handle actuator is in the closed position.
Answers which others found helpful |