FAQ Search

Can I combine M340 analog I/O modules with Telefast ABE7 sub-bases?

Using the Advantys Telefast ABE 7 pre-wired system makes it easy to install modules by providing access to the inputs (or outputs) via screw terminals. There are two specific sub-bases: Advantys Telefast ABE7CPA410 sub-base Advantys Telefast ABE7CPA412 sub-base.
FA24885  |  08-Mar-2014  | Options and Accessories
Please rate the content of this information
Unhelpful 1 2 3 4 5 Helpful
What can we do to improve this information?
 
Your email address