Search FAQs
Do I need 2 Tesys U bases (LUB12, LUB32, LUB38) for reversing operation?
The answer is no. There are multiple ways of creating a reversing starter, depending on the base module you choose. Some are built into the starter and others are add-on, but in all cases you only need one Tesys U base module.
There are 3 possible ratings for the base; 12A, 32A and 38A. Each are available in two configurations; Standard and Advanced. This depends on whether you want to use communications / advanced protection modules. Options can be found in the catalogue section, chapter A4.
You can download it here:
- Go to www.se.com
- In the search bar at the top type in A4 Tesys
- Click on the result under "documents" that says "Tesys - Chapter A4..."
- Click Download
Released for:Schneider Electric UK
Explore more
Range:
Explore more
Range: