FAQ Search

What are the functions of the Telefast ABE7CPA412 sub-base?

The ABE7CPA412 Advantys Telefast sub-base is used as a wiring interface for BMXART0414 and BMXART0814 M340 automation platform thermocouple modules.

It is used to:
  • connect 4 thermocouple probes
  • perform external cold junction compensation using the temperature sensor integrated in the sub-base and ensure continuity of shielding.
 Note: The BMXART0814 module requires 2 ABE7CPA412 Advantys Telefast sub-bases.
FA23914  |  07-Mar-2014  | Hardware Compatibility
Bookmark Print
Please rate the content of this information
Unhelpful star.gif 1 star.gif 2 star.gif 3 star.gif 4 star.gif 5 Helpful
What can we do to improve this information?
Your email address