FAQ Search

Is Ethernet communication possible with the Zelio logic modules?

Ethernet communication is possible but only with Zelio logic modular modules supplied with 24 VDC (SR 3B... BD).  The SR3NET01BD communication extension must be used. For more information on using this module, refer to the catalogue extract attached to this documentation:


zeliomodbus.pdf (PDF,1.3MB)
FA23854  |  06-Mar-2014  | Software Compatibility
Bookmark Print
Please rate the content of this information
Unhelpful star.gif 1 star.gif 2 star.gif 3 star.gif 4 star.gif 5 Helpful
What can we do to improve this information?
Your email address