FAQ Search

Is Modbus communication possible with the Zelio logic modules?

Modbus communication is possible but only with Zelio logic modular modules supplied with 24 VDC (SR 3B... BD).  The SR3MBU01BD communication extension must be used. For more information on using this module, refer to the catalogue extract attached to this documentation:

Attachment(s):

zeliomodbus.pdf (PDF,1.3MB)
FA23853  |  11-Feb-2011  | Software Compatibility
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful