Search FAQs
What is the configuration software for Lexium 05?
The configuration software for Lexium 05 servo drives was called Powersuite.
The part number of the PowerSuite software is VW3A8104 and there are two options for connecting a PC to the drive.
Option 1 - Serial
The part number of the connection kit for connecting the serial port on the PC running PowerSuite to a Lexium 05 drive is VW3A8106.
Option 2 - USB
The part number for a cable to connect the USB port on a PC running Powersuite to a Lexium 05 drive is TCSMCNAM3M002P.
Note:
Powersuite is no longer available or supported. It was software designed for Windows XP operating system and Windows NT. There was a later version of software called Lexium CT
Please use the following links, or if they are no longer working, search the Schneider website for 'Lexium CT'
For the Lexium CT software:
https://www.se.com/uk/en/download/document/LexiumCTInstall_EN/
For related documents :
https://www.se.com/uk/en/search/lexium+ct
Lexium CT on Windows 7 (64 Bit) - Internet Installation Required:
Windows 7 64Bit 1Gb RAM
Lexium CT Version 02.00.06
M1 Version V2.003 release 15.10.2008
M2 Version V2.010 release 23.12.2010
M3 Version V01.02 IE00 build 1345
This is quite old software also and we can't guarantee that it will work on Windows 10.
It does however use the Same cable as SoMove - TCSMCNAM3M002P
SoMove is the latest software that we use for the Lexium servo drives (Lexium 28, 32 and so on), but it does not work with Lexium 05 range.
The Lexium 05 series is no longer a current product. The Lexium 32 is the product range that can be used as an alternative, however there are major differences between these two ranges, in the product and the associated motors, cables and accessories.
The part number of the PowerSuite software is VW3A8104 and there are two options for connecting a PC to the drive.
Option 1 - Serial
The part number of the connection kit for connecting the serial port on the PC running PowerSuite to a Lexium 05 drive is VW3A8106.
Option 2 - USB
The part number for a cable to connect the USB port on a PC running Powersuite to a Lexium 05 drive is TCSMCNAM3M002P.
Note:
Powersuite is no longer available or supported. It was software designed for Windows XP operating system and Windows NT. There was a later version of software called Lexium CT
Please use the following links, or if they are no longer working, search the Schneider website for 'Lexium CT'
For the Lexium CT software:
https://www.se.com/uk/en/download/document/LexiumCTInstall_EN/
For related documents :
https://www.se.com/uk/en/search/lexium+ct
Lexium CT on Windows 7 (64 Bit) - Internet Installation Required:
Windows 7 64Bit 1Gb RAM
Lexium CT Version 02.00.06
M1 Version V2.003 release 15.10.2008
M2 Version V2.010 release 23.12.2010
M3 Version V01.02 IE00 build 1345
This is quite old software also and we can't guarantee that it will work on Windows 10.
It does however use the Same cable as SoMove - TCSMCNAM3M002P
SoMove is the latest software that we use for the Lexium servo drives (Lexium 28, 32 and so on), but it does not work with Lexium 05 range.
The Lexium 05 series is no longer a current product. The Lexium 32 is the product range that can be used as an alternative, however there are major differences between these two ranges, in the product and the associated motors, cables and accessories.
Released for:Schneider Electric UK
Explore more
Explore more