FAQ Search

What is the part number of the cable connecting the LTMR controller and the LTMCU operator control unit?

The LTMCU operator control unit can be connected to the LTMR controller by means of three Schneider cables with the following part numbers:

VW3A1104R10, length: 1 m
VW3A1104R30, length: 3 m
VW3A1104R50, length: 5 m
For distances greater than 5 metres:

FA23681  |  06-Mar-2014  | Hardware Compatibility
Bookmark Print
Please rate the content of this information
Unhelpful star.gif 1 star.gif 2 star.gif 3 star.gif 4 star.gif 5 Helpful
What can we do to improve this information?
Your email address