Simulation of a fault on one of the 2 valve flaps (dynamic monitoring) managed by an XPSPVK
The presses used for the cold working of metals must be routinely and regularly checked.
This check also affects the safety function provided by the XPSPVK Preventa module: faults must be simulated in order to test this function.
Method used to check the dynamic monitoring of the dual body valve when this is performed by an XPSPVK module
Caution: These tests must be carried out by suitably trained personnel.
Tests to be performed during periodic checks
1/ Equipment required for these tests

3/ Prior to the slide stopping at the upper threshold, simulate the closing fault of one of the 2 valve disks



Remove the strap after the slide has stopped at the upper threshold
Result: During positioning of the strap, the hold function for raising the slide is stopped (open output 13-14) and control of the next cycle must be inhibited via open output 21-22. In order to start a new cycle, the reset button (between terminals 7 and 8) must be operated.
Appendix

This check also affects the safety function provided by the XPSPVK Preventa module: faults must be simulated in order to test this function.
Method used to check the dynamic monitoring of the dual body valve when this is performed by an XPSPVK module
Caution: These tests must be carried out by suitably trained personnel.
Tests to be performed during periodic checks
1/ Equipment required for these tests
- Flat blade screwdriver
- Piece of insulated electrical cable, min. length 6 cm (internal voltage 24 VDC)

3/ Prior to the slide stopping at the upper threshold, simulate the closing fault of one of the 2 valve disks



Remove the strap after the slide has stopped at the upper threshold
Result: During positioning of the strap, the hold function for raising the slide is stopped (open output 13-14) and control of the next cycle must be inhibited via open output 21-22. In order to start a new cycle, the reset button (between terminals 7 and 8) must be operated.
Appendix

Answers which others found helpful |