What replaced XPSAPF? What are the differences between XPSAPF and the new XPSAK?
XPS-APF Replaced by XPS-AK
XPSAPF (old model) XPSAK (new model)

- XPS-AK has 2 extra solid state output for PLC signalling
- XPS-AK has choice between 2 models with or without removable plug terminals (P)
- XPS-APF had 3 extra N/O safety outputs
- XPS-APF could be used for Type III A two-hand control monitoring
Schematic Comparisons
Monitoring of E-stop with 2N/C contacts

Monitoring of safety mat with E-stop button


NOTE: Data sheets about new safety relays XPSAK are available on the web site to download, use the search engine (top right corner)
Monitoring of safety mat with E-stop button
Cross Reference Table
NOTE: Data sheets about new safety relays XPSAK are available on the web site to download, use the search engine (top right corner)
See also FAQ number FA141633
Answers which others found helpful |