Search FAQs
What replaced XPSAX? What are the differences between XPSAX and the new XPSAC?
The XPSAX was replaced by the XPSAC, you can see these pictured below.
XPSAX (old model) XPSAC (new model)
The main differences are as follows: - XPSAC has a solid state output for PLC signaling
- XPSAX has one additional N/C output
- XPSAC has larger range of supply voltage selection
- XPSAC has choice between 2 models with or without removable plug terminals (Add 'P' to the end of the part number)
Schematic ComparisonsMonitoring of E-stop with 2N/C contacts
Monitoring of E-stop with 1N/C contact
Cross Reference Table
Datasheets for the XPSAC safety relays are available on the website to download, just enter the part number into the search bar at the top of the page.
Datasheets for the XPSAC safety relays are available on the website to download, just enter the part number into the search bar at the top of the page.
Please note - most of the XPS relays have been replaced by XPSU, although some may still be available to purchase for a limited time. You can find information on the newest range on our website, just enter XPS Universal in the search bar.
Released for:Schneider Electric UK
Explore more
Explore more