Which network Protocols are supported on the Modicon STB distributed I/O?
The following network interface modules are avilable for the Modicon STB distributed I/O system
Ethernet Modbus TCP/IP
STB NIP 2311 dual port Standard network interface module
STB NIP 2212 single port Basic network interface module
EtherNet/IP
STB NIC 2212 Standard network interface module
CAN fieldbus
STB NCO 1010 Basic network interface module
STB NCO 2212 Standard network interface module
Modbus Plus
STB NMP 2212 Standard network interface module
Fipio
STB NFP 2212 Standard network interface module
INTERBUS
STB NIB 1010 Basic network interface module
STB NIB 2212 Standard network interface module
Profibus DP
STB NDP 1010 Basic network interface module
STB NDP 2212 Standard network interface module
DeviceNet
STB NDN 1010 Basic network interface module
STB NDN 2212 Standard network interface module
Answers which others found helpful |