FAQ Search

Can I have power factor correction capacitors inside Motorpact

Yes, power factor correction capacitors can be incorporated into the Motorpact cubicle. They are usually located alongside the main contactor for: -
  • DOL starters
  • Auto transformer starters
They will normally be in a separate cubicle for softstarters aligned alongside the softstarter cubicle.

The size of capacitors will depend on the motor size and level of power factor correction required. The capacitors will be individually protected by HV fuses.

For more information on Motorpact please click here 
FA132489  |  16-Jun-2011  | Technical Documentation
Please rate the content of this information
Unhelpful 1 2 3 4 5 Helpful
What can we do to improve this information?
 
Your email address