Search FAQs
Is it possible to mount a ZB5 head on an XACA pendant control station?
No, it is not possible to mount a ZB5 head on an XACA pendant control station. Only the dedicated XACA**** booted operators and ZA2B type pushbuttons, switches and pilot lights can be used with the XACA pendant control stations.
This is because the ZB5 has not been designed for use with the specific contact blocks used in the XACA pendant (e.g. ZB2BE101, ZB2BE102, XENG****).
It is not possible to mount contact blocks ZB2BE101 from the old ZB2 (XB2) range or the ZA2 (XA2) range on heads in the current Harmony ZB4 (XB4) metal or ZB5 (XB5) plastic range.
Released for:Schneider Electric UK
Explore more