Search FAQs
Can the cassette used to connect the circuit breakers to the Powerpact 4 panelboards be ordered separately?
No, the cassette is factory fitted only to the MGP... range and PP4.... range of circuit breakers. For example MGP1003X or PP42504X references.
If you require a circuit breaker that's not available in the standard MGP... or PP4 .... offer, for example with a different trip unit, you will need to order the cassette and breaker together along with a separate trip unit.
If you require a circuit breaker that's not available in the standard MGP... or PP4 .... offer, for example with a different trip unit, you will need to order the cassette and breaker together along with a separate trip unit.
Released for:Schneider Electric UK
Explore more
Explore more