{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can the cables used with XY2CH and XY2CE emergency stop trip wire switches be turned through angles or must they be straight?

The cables used to operate  XY2CHxxx and XY2CExxx emergency stop cable pull switches may be installed turning through angles by using the specified pulleys (XY2CZ708). There are two important rules to follow:
  • Maximum number of angles / deviations: 2
  • Combined sum of the two internal angles must be equal to or greater than 180°. See below diagram taken from the instruction sheet:

image



Caution: This FAQ references XY2CH and XY2CE only. Other rules apply for other XY2C ranges.