Search FAQs
Can I use a "conventional" limit switch for safety applications?
Yes, it is possible to use a "conventional" limit switch (i.e. non-safety specific) for safety applications, as long as the switch is "positive action"
Definition of positive action:
- A limit switch is said to be positive action if its normally closed (NC) contacts can be changed to the open position with certainty
- The symbol indicating this type of operation is an arrow in a circle.
Contact with Positive Opening
Notes:
Other conditions may be necessary for integrating a limit switch in a safety application:
- Redundancy of contacts of NC contacts
- Integrity of the sensor, the contacts in the sensor must not be modified.
For these reasons, it may still be useful to use a specific safety switch. We used to sell a range for this purpose that could be recognised by its red colour. They had a plate that prevents access to the screws. This plate was attached using "5 lobe torque" safety screws, with a special fixing tool supplied with the product. We no longer sell sensors and limit switches. For information on the above, please contact telemecaniquesensors.
Released for:Schneider Electric UK
Explore more
Explore more