Search FAQs
What are the functions of the Telefast ABE7CPA412 sub-base?
The ABE7CPA412 Advantys Telefast sub-base is used as a wiring interface for BMXART0414 and BMXART0814 M340 automation platform thermocouple modules.
It is used to:
It is used to:
- connect 4 thermocouple probes
- perform external cold junction compensation using the temperature sensor integrated in the sub-base and ensure continuity of shielding.
Released for:Schneider Electric UK
Explore more
Explore more