Search FAQs
Is Ethernet communication possible with the Zelio logic modules?
Ethernet communication is possible but only with Zelio logic modular modules supplied with 24 VDC (SR3B... BD).
The SR3NET01BD communication extension must be used.
For more information on using this module, refer to the catalogue extract attached to this documentation:
The SR3NET01BD communication extension must be used.
For more information on using this module, refer to the catalogue extract attached to this documentation:
Released for:Schneider Electric UK
Attachment(s)
Explore more
Range:
Explore more
Range: