Search FAQs
How can I find a lost code on Sepam 2000?
To find the lost code on a Sepam 2000 prior to 96/49:
go to the control logic in which the code (password) is given
To find the lost code of a Sepam 2000 later than or equal to 96/49, there are 2 options:
If the code has not been modified using the Pocket PC:
Note: The standard code (password) for the control logics is 6543210.
go to the control logic in which the code (password) is given
To find the lost code of a Sepam 2000 later than or equal to 96/49, there are 2 options:
If the code has not been modified using the Pocket PC:
- go to the control logic in which the code (password) is given.
- re-load the control logic using LOGIPAM making a note of the code (password) used.
Note: The standard code (password) for the control logics is 6543210.
Released for:Schneider Electric UK
Explore more